7/9/2016 11:22 PM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hello Olaseni, please have a look: https://support.industry.siemens.com/tf/ww/en/post/537026/ You have to call Siemens dep. near you |
7/10/2016 4:40 AM | |
Posts: 124 Rating: (13) |
Hello Olaseni, If you have a generator, certanly it must have a control panel and probably a circuit to monitor the public power to start automatically in case of fault. In addition, you need a double switches that work mechanical and eletricaly interlocked. The switching must be controled by the generator monitor circuit. To use a LOGO no more than 6 blocks is needed to do this, but I really don't recommend for this case. The generator provider has to give you support. But if you alone in this battle, let us know. We can help you. See attachement Regards AttachmentEletrical diagram 09 07 2016.zip (272 Downloads) |
Last edited by: Dinos at: 7/10/2016 4:42:45 AM |
|
7/11/2016 7:38 AM | |
Posts: 124 Rating: (13) |
Hello Olaseni, For your first requirement: See attachment. Suggestion for automatic operation. And any worker can starts the generator manually. You must have a nobreak for Logo and It is recommendable to use a three fase voltage monitor for PPS, because you certanly have all types of fault. And so I am considering both switches have coils. For your second requirement: You need a internet connection, and the Logo App installed in your cell phone. With these, only settings will be necessary. Regards, AttachmentGenerator energy supply 11 07 2016.zip (263 Downloads) |
This contribution was helpful to1 thankful Users |
7/14/2016 12:27 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
New question published by rhino1972 is split to a separate thread with the subject WinCC runtime on my Plantweb server, no "real time" display on all the inputs. Best regards |
9/12/2016 10:54 AM | |
Posts: 9 Rating: (0) |
Thank you How do I reference the timer mode. It only allows me to set a fixed time |
9/12/2016 11:10 AM | |
Joined: 12/18/2014 Last visit: 9/22/2024 Posts: 33812 Rating: (4201)
|
There's a nice FAQ from Siemens. |
Follow us on