Industry Online Support
Technical Forum
5/30/2011 12:39 PM | |
Posts: 6 Rating: (0) |
I have configuered a Thin Client using RDP connection. However the resolution of the thin client terminal is smaller than the server PC . So the screens need to be scrolled . As per as the manual attached "35122024_Thin_Client_Application_posibilities_V1_0_e" it is clearly written that for RDP connection - the resolution of the WinCC display can be changed automatically to the resolution of the thin client so that the full picture can be displayed without the need of the scrollbar. But I am not able to find any settings for enabling the autoscalibilty option in case of a RDP connection. The manual attached "hmi_thin_client_pro_operating_instructions_en-US_en-US" shows the screenshots for a RDP connection and Smartaccess connection. As per it autoscalability is supported by Smartaccess connection , however theres no such option for RDP connection. Please help me and let me know if autoscalability function is there for thin clients configured via RDP connection. AttachmentAttachment.zip (95 Downloads) |
5/30/2011 12:51 PM | |
Posts: 487 Rating: (36) |
Normaly you can set the screen size in the parameters of the RDT , see picture. |
Follow us on