2/27/2008 9:00 AM | |
Joined: 10/19/2005 Last visit: 11/30/2020 Posts: 1611 Rating: (121) |
Hi, yes this are possible. Use a MP377, make from this a backup and then you can send your customer the CF Card with the Backup-Data. Info about this you will find it in the manual. -> http://support.automation.siemens.com/WW/view/en/26248558 regards, |
2/27/2008 9:04 AM | |
Joined: 4/24/2006 Last visit: 9/20/2024 Posts: 8742 Rating: (1168) |
Dear Priscella, |
2/27/2008 7:46 PM | |
Posts: 17 Rating: (0) |
Yea I saw that too. But has anyone tried it and does it work well? To me, it seems like MPs are very dependent on the Wincc Flex software. |
2/28/2008 9:55 AM | |
Joined: 4/24/2006 Last visit: 9/20/2024 Posts: 8742 Rating: (1168) |
Hi, It should work, in my Opinion it backs up the project and CE image. Best regards, Wizard |
1/16/2009 5:26 PM | |
Posts: 14 Rating: (0) |
I did not think the CE data would back up in this manner with a USB thumb drive. If it does then this is something that I could use alot in the future. |
Follow us on