Industry Online Support
Technical Forum
10/20/2009 3:17 PM | |
Posts: 24 Rating: (0) |
Thanks for reply I have aquestion when I upload the program the symbols not appeared is it aproblem ?! best regards |
10/20/2009 3:48 PM | |
Joined: 5/28/2008 Last visit: 4/15/2024 Posts: 4505 Rating: (835) |
Dear masobhy86, No there's no problem. As if you make a program with symbols and download it to a CPU, Symbol tables does not being downloaded to it. So when you upload the software, you won't found symbol table. If you are uploading software for bck up purpose, then there will no problem as the software will work too. Think like the CPU. if you have a program with symbols and the same program without symbols. Now you are downloading the first program, The CPU will recieve a program without symbols. If you downloaded the second one, the CPU will recieve a program without symbols too. So in both cases, the same result will happen. So no problem. Regards, |
Ayman Elotaify |
|
10/21/2009 10:28 AM | |
Posts: 24 Rating: (0) |
Great thanks to reply Again and for ever thank you |
Follow us on