3/7/2020 10:23 AM | |
Joined: 12/18/2014 Last visit: 5/6/2024 Posts: 32974 Rating: (4076)
|
No, this is not possible because the parameters MinValue and MaxValue cannot be changed during runtime. |
3/7/2020 10:32 AM | |
Joined: 12/18/2014 Last visit: 5/6/2024 Posts: 32974 Rating: (4076)
|
I'm sorry, but there is no other answer ... |
3/8/2020 12:01 PM | |
Joined: 2/22/2008 Last visit: 5/6/2024 Posts: 2698 Rating: (206) |
If you need a solution for your problem, then see the example in attachment. The bargraph will start and end with adjustable parameters. Sometimes it's better to have a look from the other side. Scaling the bargraph is fixed by parameter, when you create the program. Therefore use a fixed bargraph from e.g. 0 to 1000 and normalize the display value to the same area. Regards, Scorp AttachmentAdjustable bargraph.zip (93 Downloads) |
Last edited by: Scorp at: 03/08/2020 15:16:20 |
|
Follow us on