Industry Online Support
Technical Forum
11/29/2013 12:29 AM | |
Joined: 9/27/2006 Last visit: 9/22/2024 Posts: 12282 Rating: (2684)
|
Hello swedelearner; So many questions, so little space to answer... On a S7-313 you have only one time cyclic OB, OB35, so yes that is where the FB41 (PID continuous block) must be called, and the CYCLE parameter must correspond (or be a multiple of) the cycle time set for OB35 in the CPU properties. This ensures that calculations for the PID are carried out in sync with return measurements; if you do noit do this the PID will operate erratically. The rest of the program should be called either as part of, or from OB1. You can use FCs or FBs, and use DBs to store the parameters and results of calculations for your program. If any of this seems obscure, start by looking at these manuals: Getting Started Working with STEP 7 And then open this link to tutorials prepared by Siemens for the S7-300; if you use Step 7 v. 5.5, open the link to Classic Tutorials, if you work with TIA portal, open the link to the TIA Portal tutorials, This is the best preparation you could get, to my knowledge: https://www.automation.siemens.com/mcms/sce/en/advanced_training/training_material/download_training_material/Pages/Default.aspxHope this helps, Daniel Chartier |
This contribution was helpful to2 thankful Users |
11/29/2013 5:39 AM | |
Joined: 1/28/2009 Last visit: 9/10/2024 Posts: 6849 Rating: (1365)
|
Hello, Besides what has been shared by Daniel, I will provide some clues for PID controller part.There is a powerful search facility that helps us to find previously discussions on similar issues.
And many similar issues on practical tips while using controllers can be searched in STEP 7 Additional Software Conference. Hamid Hosseini
I hope these comments help |
Last edited by: hdhosseini at: 11/29/2013 7:32 PM// typo |
|
This contribution was helpful to2 thankful Users |
Follow us on