Industry Online Support
Technical Forum
8/19/2011 11:17 AM | |
Joined: 10/13/2008 Last visit: 11/11/2022 Posts: 41 Rating: (2) |
Hi Experts, I have attached a test recipe in here and these are the details: image 1 - temperature phase was aquired and is running image 2 - temperature is in ready to complete and ticked as continuous thats why it turned to blue image 3 - the recipe is finished so its waiting for the completed status from the phase but it is still running because of the continuous function image 4 - at some time it goes to fault which says error on acquiring the phase..but it was completed.
Phase bits status: ENASTART = 1 SELFCOMP = 0 SELFRESET = 1 Question: Is this configuration possible for batch? should the termination of recipe terminates the continuous non self-completing phase? If you ask me why i tick continuous if I want it to end, is just because our client has a recipe which has a similar case and I just simplified it I have Simatic Batch V7.1 SP1 for your info If you need more details please let me know. Thank you very much for your supports Regards, mhike AttachmentTest_Recipe.zip (33 Downloads) |
Last edited by: mhike at: 8/19/2011 11:20 AMLast edited by: mhike at: 8/19/2011 11:19 AM |
|
Follow us on