7/19/2021 10:24 AM | |
Joined: 3/14/2008 Last visit: 9/25/2024 Posts: 2097 Rating: (938)
|
Hi, I see what you are trying to do. Make sure that UNIT_PLC blocks do not appear in "shortcut" folders. You need to remove shortcuts from second AS project and then synchronize with the first AS project. This will change the shortcut from second to first project. In the second AS project the UNIT_PLC blocks can be placed. Now Batch will succeed. PS: When you right click a folder, go to Plant Hierarchy and select: Remove shortcut. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to2 thankful Users |
Follow us on