4/21/2009 4:26 PM | |
Joined: 9/27/2006 Last visit: 5/6/2024 Posts: 12257 Rating: (2666)
|
Hello guys; Unfortunately, Step 7 Lite is designed for centralised I/O configuration only, on S7300 level CPUs. STEP 7 Lite is designed for traditional PLC applications with centralized I/O. STEP 7 Lite is designed for non-networked automation applications using the SIMATIC S7-300 PLC, the C7 all-in-one PLC and HMI, and the intelligent CPUs of the ET200 distributed I/O family. [From the step 7 Lite presentation page]. Basically that means no remote I/O over Profibus-DP, and no Ethernet CPs; MPI is only used for programming the CPU, no Global Data or S7 functions available. No FM modules eitherYou need Step 7 Basis (or Professional)for this type of configuration. Maybe the table found on the link below can help you sort out the issue: Differences between Step 7 Lite, Step 7 Basis and Step 7 Professional: http://www.plcdev.com/step_7_lite_professional_differences Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
4/21/2009 4:39 PM | |
Posts: 4 Rating: (0) |
Ach... as I suspected.Where can I get the Step 7 basic? Is it available for free or do I have to pay yet another fortune to Siemens? |
4/22/2009 11:24 AM | |||
Joined: 1/4/2008 Last visit: 2/27/2024 Posts: 703 Rating: (96) |
Hello, yes basic Step7 is this order:
Regard Sydney |
||
This contribution was helpful to1 thankful Users |
Follow us on