10/14/2020 7:35 AM | |
Joined: 12/16/2018 Last visit: 4/18/2024 Posts: 67 Rating: (0) |
The F-DI module with order number 1BK00 in the hardware configuration does not have the parameter "Behavior after channel fault" in compared to F-DI module with order number 1BK02 as Attachement.does this mean that in case of an failure in one of the channels of the card, only the relevant channel will not be passive and the whole F-DI module will be passive? I used Pcs7 v8.2 with F System v6.2. AttachmentAttachement.zip (60 Downloads) |