Industry Online Support
Technical Forum
6/2/2006 2:36 PM | |
Posts: 3149 Rating: (171)
|
[quote user="Waterboy"]What is the best way to implement pop-up screens in WinCC 6.0 ? By pop-up, I mean the window screens that appear when you click on the pump or valve icon in a graphic pdl at runtime. This window screen you need to create only once and different instances of it can be called with parameter passing. We can do it with several ways like using C scripting or Dynamic Wizard - Pcture Module technology. I just wonder what is the industry best practice. I would appreciate if you guys share your ways/ views and will be great if examples are provided. Cheers. Hi normally you use faceplates or picture windows. just search the FAQ for this.: http://support.automation.siemens.com/WW/view/en/23126988 http://support.automation.siemens.com/WW/view/en/22786810 http://support.automation.siemens.com/WW/view/en/22539815 http://support.automation.siemens.com/WW/view/en/23056481 http://support.automation.siemens.com/WW/view/de/18978178 okok, some FAQ are for PCS7.... nemo |
6/2/2006 8:04 PM | |
Posts: 1275 Rating: (123) |
Here we use Picture Windows as well! We pass the parameters for the picture windows through C scripts though! Best regards, Dani |