8/24/2020 10:57 AM | |
Joined: 12/12/2016 Last visit: 4/8/2024 Posts: 640 Rating: (60)
|
Hello, I'm unsure if its possible to connect various bluetooth devices to the IOT2040 simultaneously as this might also depend on the used bluetooth module, but connecting to one device should definitely work. First step would be to build your own IOT2040 image with integrated Bluetooth support. For this, first follow the regular build instructions on here.
Then edit the following file and add the respective bluez5 packages: IMAGE_INSTALL_APPEND = “ bluez5” You can use these nodes in node-red to connect to bluetooth devices. Which Cloud do you want to send data to? BR |
Last edited by: Fe_lipe at: 08/24/2020 10:59:29 |
|