11/27/2011 2:40 PM | |
Posts: 133 Rating: (13) |
Hello, You wrote you are using the CU320-2DP so make sure you are using firmware V4.3 or higher and the CF must be the Siemens compact flash card. Nextyou can disconnect all the Drive CLiQ cablesfrom the CU320-2 and power it up with 24V. At this point it should boot up and have a green Ready light and connection with STARTER via the Profibus (or Ethernet)port. Next power down connect the Drive CLiQ cables back to the CU320-2 and repower the system and diagnose the situation. AttachmentPages from GH1_LED.pdf (350 Downloads) |
Last edited by: Drives_Coach at: 11/27/2011 2:42 PM |
|
12/7/2013 8:20 PM | |
Joined: 5/12/2006 Last visit: 9/25/2024 Posts: 22372 Rating: (3014)
|
Hello, which FW Version an which CF Card do you use? Regards Christoph |
12/9/2013 4:50 PM | |
Posts: 2 Rating: (0) |
dear christo its Siemens CF card[6SL3054-0ED00-1BA0] with V04.03.01.00 with regards K.bala
|
8/4/2014 8:49 AM | |
Joined: 5/12/2006 Last visit: 9/25/2024 Posts: 22372 Rating: (3014)
|
Which FW do you use on the CF Card and which CF Card do you use? Regards Christoph |
4/18/2016 1:03 PM | |
Posts: 24 Rating: (1) |
i have this problem too. but i dont use the cf card, with no cf card the drive was not connecting to starter v4.4? |
Follow us on