4/18/2016 4:14 PM | |
Posts: 61 Rating: (1) |
I guess it's possible via starter. You will open the old project and save with a new firmware version (4.6 in your case). Then load to the new CF card. |
4/19/2016 3:56 PM | |
Joined: 8/25/2014 Last visit: 2/12/2024 Posts: 166 Rating: (2) |
Yes it is possible in two ways. SaeedRadinFirst if you need to just copy the data of CF card. You can copy through simple CF card reader (Universal Multi card reader). It is very easy. You just change the CF card not the drive is it? if only change the Cf card you just need to copy the old CF card data to new CF card through CF card reader and it will work. second thorugh starter. go online and download the parameters. Click on rate if it is helpful. |
Last edited by: pieces at: 4/19/2016 3:57:09 PMLast edited by: pieces at: 4/19/2016 3:58:04 PMLast edited by: pieces at: 4/19/2016 3:58:41 PM |
|
4/19/2016 4:00 PM | |
Joined: 5/12/2006 Last visit: 3/28/2024 Posts: 22162 Rating: (2962)
|
but note that he change from a cu320 to a cu320-2 ! Don't copy the complete content of the old CF to the new CF! Only the USER Directory! |
This contribution was helpful to1 thankful Users |
Follow us on