12/5/2014 11:48 PM | |
Joined: 6/4/2008 Last visit: 4/17/2024 Posts: 1481 Rating: (322) |
Hi, please see section 3.20 in the Commissioning Manual available to downloadHERE The two digit code in the top left of the BOP20 is the current object number, the manual shows you how to change the current object number. You will need to know which "object" number/address your target drive is. It is most common that the CU is object No 1, any Drive-Cliq based SLM or ALM will most likely be Object No. 2 and Motor Modules will follow. Please note however, that the project programmer can set his own object addresses. Regards, Graeme
|
This contribution was helpful to1 thankful Users |
12/6/2014 10:20 AM | |
Joined: 4/10/2009 Last visit: 10/23/2023 Posts: 94 Rating: (0) |
Hi U can use the attached file to access the drive parameters. Best Regards CRS
AttachmentCu320_BOP.zip (120 Downloads) |
Follow us on