2/28/2008 10:37 AM | |
Joined: 12/8/2006 Last visit: 11/27/2023 Posts: 170 Rating: (26) |
hi osama, ----------------------------------------------------------------------- (1) using tag prefix ofthe picture window ----------------------------------------------------------------------- - using tag prefix http://support.automation.siemens.com/WW/view/en/22789386 -examplefaceplate http://support.automation.siemens.com/WW/view/de/23683810 - demo project "ampel" http://support.automation.siemens.com/WW/view/en/23689276 ------------------------------------------------------------------------------------------------------------- (2) using function "Edit > Linking > Tag connections..." in graphics designer -------------------------------------------------------------------------------------------------------------- aftercopying a wincc graphic yuo should change all tag connections: In the menu bar of the graphics designer please click -item "Edit > Select All" -item "Edit > Linking > Tag connections..." ==> the dialog "Linking of the tag Connection" is opend - choose the tab "Find and Replace" -enter the string "1A" in field "Search for" -enter the string "2A" in field "Replace with" - enter button "preview" to check - enter "Replace" to replace the tag connections ------------------------------------------------------------------------------------------------------------- (3) using SetLink()-function -------------------------------------------------------------------------------------------------------------- It is possible to link the tag to the properties of graphic objects dynamically at runtime by using SetLink or ODK function SetMultiLink() |
3/1/2008 1:46 PM | |
Posts: 6 Rating: (0) |
I sued the function edit method #2 and it works ok. Thanks for your help & My Best Regards osama |