6/19/2019 5:00 PM | |
Joined: 11/15/2017 Last visit: 9/2/2022 Posts: 87 Rating: (0) |
Hello, I have come across one of you examples from a previous post,I was hoping you could elaborate on it... I do grasp the basis of the program .I have attached the file, I was looking to use and add to it. E.g...8 hour slot ..So minutes available for machine= 480...compared to actual minutes machine has run and calculate the percentage. 100% (430minutes machine ran)/ (480minutes available)=0.8958%...89.58% looking for the simplest way to work this in as a % and bar graph display Thank you for your patience Attachmentruntime_percentage_test.zip (192 Downloads) |
Follow us on