5/25/2014 12:16 AM | |
Joined: 8/22/2011 Last visit: 4/21/2024 Posts: 52 Rating: (0) |
Hello Dear Expert Teach Team, I checked the online help for this errors messages many times but I can't fix it, please see the screen shoot of parameter r949 related to the error message 1655, The offline topology is identical with the connected hardware via Drive CLiQ , But there is different between offline and online topology please see the topology screen shoot, I replaced the DRIVE CLiQ cables but I have the same bad situation, The DMM led RDY and DC link for drv12 and drv13 it always orange even if disconnect the DRIVE CLiQ cable but for other modules RDY is Green and DC link is orange and when I disconnect the DRIVE CLiQ cable RDY go to Red, Also Please find photo of SIMOTION D LEDs as attachment, I hope this information will be helpful for more diagnostic, Could you please advice me about ? Best Regards Attachmentscreen shoot.pdf (105 Downloads) |
5/27/2014 8:40 PM | |
Joined: 8/22/2011 Last visit: 4/21/2024 Posts: 52 Rating: (0) |
Hello Dear Expert Teach Team, Everything is ok, Tahnk you very much |
Follow us on