Industry Online Support
Technical Forum
8/18/2009 2:46 PM | |
Posts: 33 Rating: (0) |
When I refer to 3 PLC's .... I am trying to work out How Siemens HMI provides redundancy if possible? Any help .. ideas? |
8/18/2009 4:07 PM | |
Joined: 5/28/2008 Last visit: 12/8/2015 Posts: 901 Rating: (136)
|
Hello Bullmeister, you only have to tell us what Panel you use... regards manfred |
8/18/2009 4:40 PM | |
Posts: 33 Rating: (0) |
Cheers Ayman for your answer Do you guys know the answer to this ..... Can Siemens HMI provide redundancy?? |
8/18/2009 9:55 PM | |
Joined: 7/2/2008 Last visit: 3/18/2024 Posts: 928 Rating: (305) |
Hello Bullmeister, 1st of all, welcome to Siemens world. 2nd,I recommend to take a look at, HMI Panels catalog. 3rd, If I just may add something to what had been mentioned by gentlemen above, it would be, What is the maximum number of simultaneously active controller connections you can configure for a panel? 4th,
I'm not sure I fully understand what you mean but if you are asking if Siemens Panels can be connected to redundant controllers (Either software redundancy or H-System), then the answer is YES for sure. If youaskifpanel itself can be redundant, you can have 2 panels communicating to the same controllers and showing the same data (and same screens if you want). BUT data archives might get different on both panels. Best regards. H-H Edit, download this video, I hope you will find it useful. http://support.automation.siemens.com/WW/view/en/21063246 |
Last edited by: H-H at: 8/18/2009 10:05 PMVideo link is added |
|
Follow us on