Industry Online Support
Technical Forum
10/25/2006 5:52 AM | |
Joined: 5/24/2006 Last visit: 11/14/2007 Posts: 93 Rating: (4) |
Hi guys, Can i configure an alarm message table to show two different alarm messages from two different servers when i'm client? If I need to see the archive message of both servers, from the alarm message table, how should i configure/set the date and time to see both? If I just only need to see one server archive message, what should I do? p.s: Sorry to ask a very basic question! Currently, only 1 server & 1 client hardware i have, so i'm not able to try and test it out! attached is the sketch which shows the system of my quesiton. Kee Attachment1Client2Servers_read alarm archive.pdf (203 Downloads) |
10/25/2006 8:42 AM | |
Posts: 3149 Rating: (171)
|
Hello, does this FAQ answer your question??? http://support.automation.siemens.com/WW/view/en/23595751 nemo |
10/25/2006 9:30 AM | |
Joined: 5/24/2006 Last visit: 11/14/2007 Posts: 93 Rating: (4) |
[:o]Thanks Nemo! I got your message. |
Follow us on