5/16/2019 5:31 AM | |
Posts: 1 Rating: (0) |
Dear support. I would like to upgrade my PLC CPU model 315-2AG10-0AB0 from version V2.0.8 to V2.6.11. The problem is I only have one SD card that came with the CPU. Can I backup the SD card using Winhex or S7Lmg to backup the original image. Then load the new firmware upgrade. After upgrade complete then load the original image back? Is that possible? Thanks Alan ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/16/2019 13:16:51New subject after splitting |
|
Follow us on