1/9/2019 10:01 AM | |
Posts: 11 Rating: (0) |
Thanks. Actually I gone through the web, but got confuse so that's the reason to take expert advice. Actually I want to connect my Siemens CPU 412-5H with the another devices say A1. A1 device consist of Modbus TCP/TP protocol. So Can I Configure CPU 412-5H port to Modbus TCP/IP and communicate with device A1? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 1/9/2019 2:39:02 PMNew subject after splitting |
|
1/9/2019 8:22 PM | |
Posts: 3093 Rating: (322)
|
When you connect a device to a redundant system, it must be capable to hold two ModbusTCP connections simultaneously. Regards, |
Follow us on