1/22/2015 7:25 PM | |
Posts: 784 Rating: (52) |
RaiMahi wrote: Hi I am using TP900 Comfort panels. I am using wincc TIA portal for HMI design.Can I store my Screens on SD card. Instead of usin PG to download screens on Panels, can I download them from SD card to Comfort panels Thanx Mahi Hello, Have a look at thislink. Murof wrote: Im Sorry You cannot make a transfer of the Panel using a SD Card Wrong Best regards.... |
11/8/2016 6:21 PM | |
Posts: 439 Rating: (108) |
Hello VVago, He specified:
Which is not the same as creating a backup and restore it. Doing a backup generate a filewith the extension *.psb. It is not possible to generate a .psb file with TIA, put it on a SD card and restore from it. Now, with TIA V14 (not earlier versions), it is completly different. You are able to transfer your project on a USB stick or a SD card and use the new "project transfer" tab in the control panel of your HMI to transfer the project. How with the TIA Portal do you transfer your project to your operator panel via a storage medium (USB stick, for example)?Best regards, Hugo |
This contribution was helpful to1 thankful Users |
Follow us on