4/6/2012 11:35 AM | |
Joined: 1/28/2009 Last visit: 4/1/2024 Posts: 6836 Rating: (1359)
|
Hello , Network ,its title and comment are a whole .They shift up or down together in case of a network removal or addition respectively.See the attachment for more evidence.As our "Diamond"member requested before, snapshots are really crucial . Please upload the source project or snapshots related to your!Best regards, Hamid Hosseini Attachmentnet.zip (43 Downloads) |
This contribution was helpful to1 thankful Users |
4/8/2012 2:12 PM | |
Joined: 10/7/2005 Last visit: 4/26/2024 Posts: 3004 Rating: (1046)
|
Hello wirenut the issue that you encountered can (well, will) happen if you for example copy and pastean FC or FB from the online program into your offline programAND that online copy had an additional Network in it. I'm afraid to say I'm not aware though of an easy or automated fixfor this problem (never really had to worry about this problem as it is - or should be - a rare occurence), but you can definetely do themanual copy/paste of Network comments in the Step 7 Editor or alternatively do it via source file editing (which may be a bit faster). I hope this helps and please let us know if you find a better way. |
Cheers |
|
This contribution was helpful to1 thankful Users |
4/9/2012 6:43 PM | |
Joined: 4/5/2006 Last visit: 8/13/2023 Posts: 642 Rating: (131) |
Hello, maybe this can help you: http://raeppel.de/tools/netzwerktiteleditor.htm http://raeppel.de/tools/commentedit.htm Regards André Räppel --------------------------------------------------------------------------------- www.raeppel.de work faster withinnovative PLC-Tools |
Follow us on