7/12/2013 3:53 PM | |
Posts: 165 Rating: (2) |
I have a tag (TagSS) showing a counter in seconds. I want to show the minutes. Can I have an I/O field showing TagSS/60 ? If so - how is it done? |
7/12/2013 4:44 PM | |
Joined: 11/21/2007 Last visit: 8/12/2024 Posts: 2325 Rating: (308) |
Hello Jake2011 It is very easy this way Right Click on "Output Value" and Select "Dynamic Dialog" Select "Direct" and create the Expression You can either type in the expression or Select "Tag" and "Operator" or "Function" using the options provided. I have attached a sample screenshot for your ready reference Hope this helps Cheers Navnag |
There is no such thing as the last bug in a program |
|
This contribution was helpful to1 thankful Users |
7/12/2013 6:45 PM | |
Joined: 11/21/2007 Last visit: 8/12/2024 Posts: 2325 Rating: (308) |
Thanks Pranav J. Bhagat Linear scaling affects the value of the basic tag and not the I/O field in the picture. It is a great tool if it is just a simple scaling. However if the idea is to display the result of an expression ( involving one or more tags ) then using the required expression as Direct Action in the Output field is a better option. e.g. if you have one Tag for Hours and another for minutes and you f=want to display total time in minutes .... Hope this helps Cheers Navnag |
Last edited by: Navnag at: 7/12/2013 6:47 PMThere is no such thing as the last bug in a program |
|
7/15/2013 1:13 PM | |
Joined: 10/3/2010 Last visit: 9/18/2024 Posts: 1561 Rating: (191) |
I think you should create a Project Module (bmo) for this starting with Sub GetBit(BitNo, Bits) End Sub |
B r g d s , |
|
7/15/2013 2:27 PM | |
Joined: 10/3/2010 Last visit: 9/18/2024 Posts: 1561 Rating: (191) |
Hey Jake, did you try to remove "Public" from your code? Did you check apdiag.exe for possible more diagnostics? |
B r g d s , |
|
Follow us on