5/29/2018 7:37 AM | |
Joined: 3/5/2014 Last visit: 2/26/2021 Posts: 4329 Rating:
|
hi, yes, there are input modules that can work as counter. for example this one, 6ES7521-1BL00-0AB0, can count up to 1 kHz frequency. There are much more modules that can count, also the compact-PLCs, 1511C and 1512C have 32 high-speed digital inputs for signals up to max. 100 kHz Have a look the technical data and the manual of the modules and PLCs. Here you can find all together in a collection: SIMATIC S7-1500/ET 200MP Manual Collection hope this helps, regards, |
There is no bad feedback! |
|
5/29/2018 8:26 AM | |
Joined: 5/6/2016 Last visit: 10/15/2020 Posts: 4 Rating:
|
Ok thanks, I am using 1515-2 PN PLC. So then i think i can use counter module for this PLC also. |
5/29/2018 10:22 AM | |
Joined: 8/31/2005 Last visit: 2/24/2021 Posts: 2071 Rating:
|
You can use to read in an encoder:
To calculate the time between two digital signals:
|
|
|
This contribution was helpful to
1 thankful Users |
7/2/2018 9:24 AM | |
Joined: 5/6/2016 Last visit: 10/15/2020 Posts: 4 Rating:
|
OK But my client dint want to use extra module for this, So can i measure speed via standard Digital input. |
Follow us on