10/21/2019 11:00 AM | |
Joined: 7/24/2014 Last visit: 12/4/2023 Posts: 392 Rating: (66) |
You can by using the GET block and then try to read the IO's of the partner CPU having Ethernet. S7-1200 and S7-400 Put and Get |
Thanks and Regards |
|
This contribution was helpful to1 thankful Users |
11/23/2019 12:08 PM | |
Joined: 7/5/2006 Last visit: 9/25/2024 Posts: 180 Rating: (4) |
Hello. Smit, i've tryed between a S7-1200 as a client and a S7-300 as a server and it's work fine. It's possible to see all the I/O area of the S7-300. The only thing that need is the IP address of S7-300 cpu's. bye |
11/23/2019 1:02 PM | |
Joined: 12/27/2018 Last visit: 9/18/2024 Posts: 510 Rating: (43) |
Refer this video.It would be helpful. |
Jinson James, M.Tech (Power Electronics and Power System), |
|
Follow us on