3/26/2018 9:21 AM | |
Joined: 4/8/2016 Last visit: 2/13/2024 Posts: 133 Rating: (45) |
Hello ckju_1026, yes, you can use the CP443-1EX30 (as hardware) and the CP443-1EX20 V2.0 (configured in HW Config). But please keep in mind that you can only use the functions which are supported with the CP443-1EX20 V2.0. This is called "Deploying new hardware as a replacement" and you can find the general description, that this is possible with PCS 7 in Compendium Part D. https://support.industry.siemens.com/cs/ww/en/view/109741659 For this case you find the information that the CP443-1EX30 (hardware) is compatible with CP443-1EX20 V2.0 in the manual of the CP443-1EX30. (Chapter 7.3) https://support.industry.siemens.com/cs/ww/en/view/59187251 |
Kind regards |
|
This contribution was helpful to1 thankful Users |
Follow us on