2/20/2020 1:23 PM | |
Posts: 152 Rating: (5) |
Hello everyone, I have one question: Can I use the licence from the USB stick without copying it to my PC? My idea is to copy all my licence on one USB stick and then just to plug it in PC when I need to work in TIA Portal. I managed to copy STEP 7 Professional and WinCC Advance licence on my USB stick but look like the TIA Portal can not read the licence from the USB stick. When I start TIA it says I do not have a licence for software, but when I open Licence Manager and when I go to this USB I can see both licences STEP7 and WinCC. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 02/21/2020 09:27:26New subject after splitting |
|
2/21/2020 9:52 PM | |
Joined: 7/7/2010 Last visit: 9/18/2024 Posts: 15204 Rating: (2417)
|
If you want something like that, you can write some scripts, perhaps using AutoIT!, that launch upon USB insertion (but most I.T. security types frown excessively at this type of suggestion for obvious reasons), and then copy all licenses to the c: from the usb drive. Then you can create an eject script that copies them all back, and then sets the usb drive ready to eject. Simple to say, and not so simple to do. It is easier to store them onto a windows server or PC that is always available that has the latest ALM installed, configured to allow moving licenses to/from it without restriction. Then you can store all your licenses on the server, and any PC that can access that license server can pull them down with ease, and put them back with ease too. No remembering to carry around the key fob. Except remember to check out any required licenses before setting off to a remote facility.
|
science guy |
|
Follow us on