5/16/2016 6:42 AM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hello Yes but first you have to migrate from Protool to Wincc Flexible (SP2) in MP 277 and after to TIA Portal Have a look Chapter 1.4 - Pag. 9 it should be KP 1200 Migration Guide Comfort Panels - Siemens |
Last edited by: Ste39 at: 5/16/2016 6:43:26 AMVersion |
|
This contribution was helpful to1 thankful Users |
5/16/2016 6:42 PM | |||
Joined: 3/28/2015 Last visit: 4/19/2024 Posts: 721 Rating: (213) |
Hello, 1-You should have the original HMI program to be able to do the migration. How do you back transfer the projects of an operator panel and what should you watch out for? 2-Migrate MP270 to MP277 using WinCC Flexible 2008 SP2 3-Migrate MP277 to KP1200 using WinCC TIA 4-
5-How can you transfer a WinCC (TIA Portal) configuration to an operator panel using Ethernet? |
||
Eng.Mohamed Ibrahim |
|||
This contribution was helpful to1 thankful Users |
5/17/2016 11:31 AM | |
Joined: 6/3/2014 Last visit: 1/17/2023 Posts: 660 Rating: (191) |
Hello Sasongko, from what I can see the most similar Comfort Panels would be the KP1200 and the KP900. It depends a bit on what you need. The old panel had 36 keys, the Comfort Panels have 34 keys(KP1200) or 26 keys (KP900). The change of the format from 3:4 to 16:9 is unavoidable with such a change, of course. While you're still planning the update - do you want to stay with a key panel or might a touch panel be more effective? Here is an overview over availiable documents/FAQs/... on migration of the HMI:
|
~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ★ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ |
|
Follow us on