7/28/2021 11:44 AM | |
Joined: 3/14/2008 Last visit: 9/17/2024 Posts: 2095 Rating: (936)
|
Hi, You need to put those addresses in the symbol list in order to use them. If you have done so, you need to use a structure composer in order to create a structured signal consisting of BOOL and ST for example. Because now you are trying to connect a hardware signal to a structure signal. APL uses structures for digital and analog signals. The structure consists of Value of type BOOL/REAL and a ST of type Byte. APL features structure blocks to create or separate structures into Value and ST. If you use FC378 from the AP library (StruDiOu), you can connect "Value" with the IO address and then connect "Out" to the Intlk02 block. Please set the ST value to 16#80. |
Last edited by: Oreca at: 07/28/2021 11:48:33Last edited by: Oreca at: 07/28/2021 11:50:49If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to2 thankful Users |
Follow us on