1/10/2020 8:50 AM | |
Joined: 3/14/2008 Last visit: 9/20/2024 Posts: 2095 Rating: (936)
|
Hi, The I/O has the attribute: S7_link:='false' meaning you cannot connect anything to it in CFC. In order to change this, do as follows: 1. Go to the block (FBxxxx) in your blocks folder and open the block. Ignore the warning. 2. In Interface, go to "IN" and find the I/O. 3. Right click the I/O and open select: Object Properties. 4. Go to tab: "Attributes" and delete the S7_link attribute or you can change it's value from false to true. 5. Click on OK and save the block. The change will effect all instances of the function block. |
Last edited by: Oreca at: 01/10/2020 08:51:23If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to2 thankful Users |
Follow us on