6/20/2014 3:18 PM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hi lolo1234, which is the code of your CPU? SF led isON or OFF? |
Last edited by: Ste39 at: 6/20/2014 3:19 PM |
|
6/20/2014 4:03 PM | |
Posts: 47 Rating: (0) |
Hello, You seems to be right. Good job I will try with lower memento thank you very much. |
This contribution was helpful to1 thankful Users |
6/23/2014 10:57 AM | |
Posts: 47 Rating: (0) |
Hello, I finally checked the number of M-bytes my CPU can hold and I think he can hold more than 256 bytes because he got additional I/O modules. you can see it on the linked file. That means that I still don't know why I can not put a FB in the program. I am answering late I hope somebody is still there . Cheers. AttachmentM-bytes.pdf (147 Downloads) |
6/23/2014 11:22 AM | |
Posts: 1064 Rating: (72) |
adding additional I/o doesn't change the memory allowed you still only have 256 mbytes available in your processor your processor is 6es7-315-2af02-0ab0 according to your screen shot here are your specs https://support.automation.siemens.com/WW/llisapi.dll/4067858?func=cslib.csinfo&objId=4067858&objAction=csView&nodeid0=33516848&lang=en&siteid=cseus&aktprim=0&extranet=standard&viewreg=WW&load=treecontent&prodLstObjId=4067855&start=271&csSort=-DOCDATUMBEITRAG&subtype=130000 |
6/23/2014 11:39 AM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hello lolo1234, CTRL+ALT+R |
6/23/2014 11:46 AM | |
Posts: 47 Rating: (0) |
Ctrl+alt+R still doesnt work . |
Follow us on