12/29/2019 8:02 PM | |
Posts: 13 Rating: (0) |
Hello Techology Team! I using CPU 1215 and inverter Sinamics V90 (6SL3210-5FE10-8UA0) i try to move servomotor simotics S-1FL6 (1FL6044-1AF61-QAB1). For it I use interface PTO. In CPU i created TO Axis_1 (Technology object) and setting all parrametrs. In "Commissicning" (see file in attachment) is possibility to move servomotor in differents modes: jog, possitiong, homming. For it, the invertor must be parametred and in CPU must be created TO Axis_1 and signal Servo ON =0 (from PLC to Invertor). I open this control panel in "Commissicning", set mode Manual control, PLC go to online mode, its Ok, than i want to press Release (number 3 on pictures in attachment), but button Release is not avvalible (is grey) and all other buttons and fields on this control pannel are not avvalible. During it CPU goes to stop. I can not move directly servomotor from PLC using standart control panel in TO of CPU 1215. What is that problem? Thans for All! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/30/2019 10:55:52New subject after splitting |
|
1/9/2020 10:39 AM | |
Joined: 4/28/2015 Last visit: 9/20/2024 Posts: 397 Rating: (56)
|
Hello, did you notice the "ready input" of drive...? For detail information, please have a look to:
|
Follow us on