1/15/2019 9:55 AM | |
Joined: 7/17/2018 Last visit: 4/9/2024 Posts: 3 Rating: (0) |
HI i have exactly same issue but with the 7VK87 and 7SL87 relay i have below eror BGTS 220kV CB106 X CBM,Required device drivers missing for this device. Import device drivers 7VK87 CFG V07.50.12,Hardware and protocols,1/15/2019,7:47:21 PM i installed V7.5 Line driver and protocol drivers but still i can not use my config file becuase of above problem i used this file recently without any problem but i delete all the drivers and installed them again but it dos'nt work after installation ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 1/15/2019 2:18:33 PMNew subject after splitting |
|
Follow us on