7/21/2018 1:23 PM | |
Joined: 8/30/2017 Last visit: 5/30/2024 Posts: 4 Rating: (0) |
Hiii, EVeryone, I already have 4 ET 200 series CPU; IM 151-8 CPU in communication, and I want to add 5th new station, S7 1200 firmware version 4.0 (MLFB no is= 6ES7-215-1HG40-0XB0),but I can't achieve communication between S7 1200 (4.0 firmware) CPU and Wincc v7.2 Runtime. Corrective actions I have taken: 1. Installed Simatic NET PC V 8.2 + SP1 2. have attached IE general in the hardware of the program and given the IP of SCADA pc to the IE general and downloaded into the S7 1200 CPU. although communication is not happening. So please guide me what next to do to achieve the communication. Here I have also attached some screenshots. Is S7 1200 IP tool necessary for communication.? with regards, Mitul SUthar ------------------------------------------------------------------------------------------ |
Last edited by: ganesha@2512 at: 7/21/2018 1:29:24 PMLast edited by: Jen_Moderator at: 7/23/2018 11:48:50 AMNew subject after splitting |
|
7/23/2018 12:01 PM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
Closed cause question posted twice.
|
Follow us on