6/21/2016 11:04 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1051) |
hi, what kind of PLC did you project? MLFB? What TIA-version do you have? V13 incl. SP1? regards, |
FCK WAR! |
|
6/21/2016 11:50 AM | |
Posts: 99 Rating: (0) |
for SMJE - im have only cpu in network, my ip adres i dont know. for mopS04 - im have tia v13 s1 update 5. Im not understand what are you mean MLFB? |
6/21/2016 12:30 PM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hello, Like 6ES7 21x-xxxxx-xxxx This is an example of MLFB regarding Micromaster: MICROMASTER 4 (MM4): Example of an article number (MLFB) - ID ... |
Last edited by: Ste39 at: 6/21/2016 12:33:58 PM |
|
6/21/2016 12:33 PM | |
Joined: 4/28/2015 Last visit: 5/6/2024 Posts: 34 Rating: (6) |
Hey, this link may help to know what is MLFB number (PRODUCT number of PLC).
Check your PC ip address first by given Image. add IP (192.168.0.10) & subnet mask (255.255.255.0) of your PG per your uploaded image, if only one PLC is in network keep in mind. Try it please. Just ping your PLC first after editing your PG ip address.
if ping is ok then try to download. Thanks.
|
Last edited by: SANDY GORASIYA at: 6/21/2016 12:36:09 PM |
|
This contribution was helpful to1 thankful Users |
6/21/2016 12:48 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1051) |
hi, Machine readable Product Designation (MLFB) or Order No. has this format: 6ES721x-xxxxx-xxxx regards, AttachmentMLFB-manual.pdf (145 Downloads) |
FCK WAR! |
|
Follow us on