3/6/2012 8:10 PM | |
Posts: 3 Rating: (0) |
Dearspecialists, I have a PCS7 V7.1 engineering station with2 ethernet cards. One card with only the ethernet protocol (plant bus) and one ethernetcard(terminal bus)with tcp/ip and the nessecary profinet protocols.(see attachment). After changing the pg/pc interface with the menu accessible nodes, i only see s7 cpu's.(see attachment). I also have a new M3 field-pg with Step 7 professional V5.5 SP1. With this field-pgI also seethe profinet devices. What doI wrong on the engineeringsstation?? Thanks for your help Attachmentscreenshots.pdf (66 Downloads) |
Follow us on