4/25/2020 5:41 PM | |
Posts: 1 Rating: (0) |
Hello everybody I creat a project in TIA & add one S7 1200 & PC station .in PC station i have a wincc runtime pro & IE general . I connect PLC with IE general in Device & Network and in Wincc runtime/ connection add S7 1200 Device And Access point is S7ONLINE . Inthe PLC in write a program with a memory and a output for test connection situation . In screens I add a screen with 2 button for set & reset the memory in PLC . But when I started simulation it's doesn't work and I can't turn on /off memory of the PLC . Please help me . Thanks for reading 🙏🙏🙏❤️ ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/27/2020 10:32:25New subject after splitting |
|
Follow us on