8/21/2014 8:58 AM | |
Posts: 1368 Rating: (126) |
Hello, Which connection type you use for connection to the PLC? Ethernet? MPI? If you use MPI, please check the parameters described here: http://support.automation.siemens.com/WW/view/de/10420976 |
8/21/2014 10:41 AM | |
Posts: 1368 Rating: (126) |
You said, after changing the MMC card, it works without errors. Do you try this mmc card (from the CPU 313) to another PLC? If it works, then , if not, the mmc card seems to be defect. BTW: another post with the same error message /tf/WW/en/Posts/103940 please check also this... |
Last edited by: Pittiplatsch at: 8/21/2014 10:44 AM |
|
8/21/2014 11:40 AM | |
Joined: 2/11/2013 Last visit: 4/18/2024 Posts: 5 Rating: (0) |
PLC is functioning with that orignal MMC Card and the machine is in operation |
8/21/2014 1:21 PM | |
Joined: 2/11/2013 Last visit: 4/18/2024 Posts: 5 Rating: (0) |
I haven't tried orignal mmc with other 313. I will be in touch after testing that. Thanks for your help.
|
8/22/2014 8:09 AM | |
Posts: 1368 Rating: (126) |
Hey, have a look at this faq http://support.automation.siemens.com/WW/view/de/19215608 or http://support.automation.siemens.com/WW/view/de/26123822 can it be, that something like this is placed in your program? |
Last edited by: Pittiplatsch at: 8/22/2014 8:16 AM |
|
Follow us on