11/12/2018 11:24 AM | |
Posts: 4 Rating: (0) |
Hi, 1. Where can we find the Help documentation on using SIMOSIM TIA 15? 2. In our projects usually we have two PLCs 1200 and Simotion D425. And there are IO communication (using I-devce) between them. Can we use PLCSIM and the SIMOSIM at the same time ? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/12/2018 1:34:28 PMNew subject after splitting |
|
11/12/2018 2:13 PM | |
Posts: 4 Rating: (0) |
I must have SIMOSIM advanced ? |
11/12/2018 2:54 PM | |
Posts: 4 Rating: (0) |
and Where can we find the Help documentation on using SIMOSIM TIA 15? |
11/12/2018 2:55 PM | |
Posts: 4 Rating: (0) |
I must have SIMOSIM advanced for OPC server? |
11/14/2018 10:01 AM | |
Joined: 10/11/2006 Last visit: 4/26/2024 Posts: 5825 Rating: (789)
|
Hello you can use OPC UA with included SIMOSIM SIMOTION. The OPC-UA Server can be configured via IT-Diag (SIMOTION Web-pages) . Please note: for using OPC-UA with SIMOTION V5.2 with device D4x5-2 you can select the Port (example X127...) in WebPage. If using OPC UA in SIMOSIM you have to do a config-setting in WebCfg.xml File Endpointuserdescription: Ur= " opc.tcp://TCP/IP adr. :Port No"/ and the certificate have to be copy.(this is only necessary when using OPC-UA in SIMOSIM) In next version SIMOTION V5.3 the configuration can be done also in Web. Without any changes in some configuration files. please note, |
With best regards, |
|
Follow us on