Industry Online Support
Technical Forum
7/4/2012 11:07 AM | |
Posts: 3037 Rating: (192)
|
Hello, You can find more information about script. How do you dynamize objects in WinCC flexible via scripts? Which VBS information and programming aids are there in WinCC flexible? If you want create a message with script, then you can use the function "ShowSystemAlarm". Which properties want you display of discrete alarm? Tweety |
7/11/2012 3:18 PM | |
Posts: 3037 Rating: (192)
|
Hello Ray Huang, You can not accessto properties ofa discrete alarm from a script of WinCC flexible. Tweety |
7/12/2012 9:32 AM | |
Posts: 12 Rating: (0) |
I see. I guess I need to use some indirect approach to make it. Thank you Tweety. |
Follow us on