7/8/2013 2:33 PM | |
Joined: 8/25/2006 Last visit: 9/18/2024 Posts: 2209 Rating: (278)
|
Hello. It is not possible to use FM458 without S7-CPU, you can't compile HW Config in this case. You can connect WinCC directly to the FM458-1DP only (not FM458) over DP, IE (if you have IE-CP in the rack) or MPI, this is described in themanual, chapter 4.9.
|
This contribution was helpful to1 thankful Users |
7/8/2013 3:03 PM | |
Joined: 11/21/2007 Last visit: 8/12/2024 Posts: 2325 Rating: (308) |
HelloKSN I was trying to see if we can cut some cost in our configuration by saving the CPU. Thanks Navnag |
There is no such thing as the last bug in a program |
|
8/21/2013 1:22 PM | |
Joined: 5/22/2012 Last visit: 3/24/2022 Posts: 895 Rating: (67) |
Hello Navnag, if you use a SINAMICS S120 drive, some of the FM458 blocks are available there - for example: http://support.automation.siemens.com/WW/view/en/72839973 But that depends on your application. A direct HMI access to to S120 (without PLC) would be possible (also with Panels which are only avaible in the TIA Portal). Further it would be possible to write own C/C++ blocks and use it on a S120. But in the first step only from the SIEMENS application centers. Regards Zako |
This contribution was helpful to1 thankful Users |
Follow us on