12/15/2018 11:19 PM | |
Joined: 10/26/2015 Last visit: 2/1/2023 Posts: 15 Rating: (1) |
Hi guys I have spend a lot time this already. Irs my brain in. Please help My configuration is as follows: OS1- Primary OS2 - Standby ES/OC In OS2, I can't add archived tags into runtime trends or offline trends. When I open up online trend control and select archive tags in data source and click on tag I get the window in Pic-1 (see attachment). If I do the same in OS1 I get the window in Pic-2 from which I can select the tags I want This is same irrespective of the redundancy status of the servers. In ES/OC, I can always pick the archive tags from the server even when OS2 is the main server (Pic-3). There is no problem in selecting online tags in OS1. The pre-configured trends (configured in ES and downloaded) are working fine and if I manually type in the tag in the format <ArchiveName>\<tagname> in OS2, it will start logging normally Taglogging is enabled for OS2 PC TagloggingFast and Tagloggingslow DBs are updating in the ArchiveManager folder in the project folder. checked task manager and cctlgserver.exe is running AttachmentPics.pdf (62 Downloads) |
Follow us on