11/12/2015 7:17 AM | |
Posts: 72 Rating: (0) |
Dear Expert, I have a problem with communicate between PLC and wincc Runtime on PC. CPU 1214 DC/DC/DC : 6ES7-214 1AG40 - 0XB0 FIRMWARE V4.0 My software is Wincc Advanced v 13.0 sp1. I can download program and monitor PLC can modify bit ... , but when i start wincc runtime , it seem that i cannot communicate with plc although i've already set the PG/PC interface. Please refer the attached file to see if sthing goes wrong. Thank in advanced. AttachmentTest.rar (1252 Downloads) |
11/16/2015 7:34 AM | |
Posts: 72 Rating: (0) |
Hi ChristophD, I'd like to say thank for your help, Now it works. Thank you so much. |
This contribution was helpful to1 thankful Users |
Follow us on