Industry Online Support
Technical Forum
5/29/2013 9:06 AM | |
Posts: 40 Rating: (0) |
Dear all, I am using winc flexible 2008. Untill yesterday it was running fine but now it is showingcannot connect to configured SQL server.....plz help.......
|
5/29/2013 10:28 AM | |
Posts: 3037 Rating: (192)
|
Hello, Have a look in the following link. What are the possible causes of an unsuccessful Microsoft SQL Server 2005 Express installation or why is creating or opening a WinCC flexible 2008 project aborted? Tweety |
9/12/2013 10:31 AM | |
Posts: 53 Rating: (2) |
Hello, i have the same problem. I tried the solution described above, but without result ... Still the same problem ... Pls help. Henio.
|
9/17/2013 11:06 AM | |
Posts: 3037 Rating: (192)
|
Hello, You must do the point 1.4 in the following link. http://support.automation.siemens.com/WW/view/en/29420407 Tweety |
9/17/2013 12:59 PM | |
Posts: 53 Rating: (2) |
Hello, as i said, i did, but without positive result ... still the same problem. Henio.
|
9/17/2013 4:27 PM | |
Posts: 3037 Rating: (192)
|
Hello, I found this link from microsoft. http://social.msdn.microsoft.com/Forums/sqlserver/en-US/9e01e870-0bff-4669-a385-2d9349b1a4f0/error-15372-on-adding-new-sql-database-in-vwd Do you delete all folders under this path? %USERPROFILE%\AppData\Local\Microsoft\Microsoft SQL Server Data\WINCCFLEXEXPRESS See the point 2.1 http://support.automation.siemens.com/WW/view/en/29420407 Tweety |
9/18/2013 10:21 AM | |
Posts: 3037 Rating: (192)
|
|
Follow us on