6/22/2017 10:25 AM | |
Posts: 648 Rating: (95) |
Hi S. Veselinov, manual: SDB > 1000: hardware configuration, in offline project not available Did you Update your system? First make a update. It could be possible, that one or more hardware components need much more time for RUN. As result the CPU goes in modus STOP.
As a other alternative do the following: Therefore this link could be helpful: If this doesn't help contact the technical support and make a service request. https://support.industry.siemens.com/My/ww/en/requests With best regards rh1990 |
6/29/2017 11:16 AM | |
Joined: 12/28/2015 Last visit: 1/24/2024 Posts: 256 Rating: (26) |
Hello what did you mean with remotely? A WinCC Professional project can be transferred via download. See the following Chapter 3.3 in this document https://support.industry.siemens.com/cs/ww/en/view/109745023 Another way is that you take the compiled file from your engineering pc and take that to your runtime pc. And then start the project with WinCC RT Start. |
Follow us on