8/19/2012 3:47 PM | |
Joined: 10/15/2010 Last visit: 4/3/2024 Posts: 36 Rating: (0) |
Hi I've just installed software PCS7 V7.1 SP4 to my new ES. However, I can't find the new CPU S7-414-5H on the hardware config. The current installed software modules is attached. STEP7 version is 5.5 HF6 Do I have to installl the service pack1 and hotfix1 below to the STEP7 be able to configure S7-414-5H ? http://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=59216386&caller=view Because, this is PCS7 ... I'm not sure that we can manually update the service pack and hotfix to the STEP7 or not? Please kindly recommend the proper method to configure PCS7 V7.1 SP4 to use with 414-5H Thank you. AttachmentInstalled SIMATIC products.pdf (111 Downloads) |
8/20/2012 10:46 AM | |
Posts: 836 Rating: (99)
|
According to the release notes this CPU should be supported. Have you done the installation of SP4 according the readme file? |
8/20/2012 2:47 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello, Yes, there is mention that CPU414-5H (not 6.0) is released to use in 7.1 SP4 but it should
So, version 6.0 is available from 8.0 Update1. Anyway my suggestion isSupport Request. Do not use above mentioned HF in case of PCS7. Best regards, Hristo Mihalev
|
8/20/2012 4:08 PM | |
Joined: 10/7/2005 Last visit: 3/18/2024 Posts: 2 Rating: (1) |
Hello, |
8/3/2015 1:05 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
|
Follow us on