(2)| 2/12/2009 4:10 PM | |
|
Posts: 3149 Rating:
|
Hi - which other software is installed? - in which sequence did you install your software? - which user rights do you have? - are there any entries in the diagnose files (..\wincc\diagnose)? http://support.automation.siemens.com/WW/view/en/21947334 nemo |
| 8/11/2009 8:36 AM | |
|
Posts: 34 Rating:
|
The /console option has been removed in XP SP3. You now have to use /admin to connect from an XP SP3 machine to the console session. |
| 3/15/2014 6:57 PM | |
|
Posts: 17 Rating:
|
Good afternoon. When you create a project WinCC 7.2 gives an error "Cannot open or start WinCC project, as Project Manager cannot start basic application XREF". Operating system WinXP SP3. In the beginning it was established Step 7 5.5, then WinCC 7.2, Step v12. In the application of a diagnostic file. What can be done? In a system with administrator privileges. AttachmentPMStart.zip (494 Downloads) |
Last edited by: Serega77 at: 3/15/2014 7:02 PM |
|
| 3/17/2014 11:09 AM | |
|
Posts: 821 Rating:
|
Hi, do you also use remote desktop? Best Regards, Healthcheck |
| 7/15/2014 11:49 PM | |
|
Posts: 176 Rating:
|
New question split intoProject Manager can't start basis application XREF using Wincc V7.0+Sp3 on a windows 7 PC. With best regards, Narrator1
|
Follow us on