5/1/2008 11:11 PM | |
Posts: 2661 Rating: (279) |
_njoy: |
5/1/2008 11:49 PM | |
Posts: 2661 Rating: (279) |
Do you get an error message after download is complete? May be there is a lock file (LCK) that needs to be deleted. Did you see the following FAQ's? I found them very useful while troubleshooting server problems. After reloading the OS project to the server from the ES, how do you clear the undefined error message and the abort? http://support.automation.siemens.com/WW/view/en/22019649 How can you clear the error message "Download (310:88)"? http://support.automation.siemens.com/WW/view/en/22559073 Which messages may appear in the "Download OS" dialog box? http://support.automation.siemens.com/WW/view/en/26460192 How do you use the SIMATIC shell to configure the terminal bus of a WinCC station? http://support.automation.siemens.com/WW/view/en/25437381 |
5/2/2008 4:08 PM | |
Posts: 29 Rating: (0) |
If other tries won't work, first thing in the morning. Thanks! |
5/2/2008 5:39 PM | |
Posts: 29 Rating: (0) |
Just tried with a new project/new OS. Same story. It seems to me that only option left is to re-install the server. |
Follow us on